*** Errors ***

34	  1> *** The DUT delayed 314 ms to respond to the unicast ListIdentity command. The DUT shall not delay to a unicast ListIdentity request. Please verify the actual delay with a Wireshark capture.
144	  2> *** sendto() failed with error: A socket operation was attempted to an unreachable network.
154	  3> *** ListIdentity Failed
2718435	  1> *** The DUT delayed 316 ms to respond to the unicast ListIdentity command. The DUT shall not delay to a unicast ListIdentity request. Please verify the actual delay with a Wireshark capture.
2718475	  2> *** The DUT delayed 308 ms to respond to the unicast ListIdentity command. The DUT shall not delay to a unicast ListIdentity request. Please verify the actual delay with a Wireshark capture.
2722188	  1> *** The DUT delayed 339 ms to respond to the unicast ListIdentity command. The DUT shall not delay to a unicast ListIdentity request. Please verify the actual delay with a Wireshark capture.
2722244	  2> *** After Type 0 Reset, no DUT response at new address 192.168.1.11. Is Reset timer not long enough?. (NV value not maintained ?)
2722253	  3> *** The DUT delayed 310 ms to respond to the unicast ListIdentity command. The DUT shall not delay to a unicast ListIdentity request. Please verify the actual delay with a Wireshark capture.
2722269	  4> *** After Type 0 Reset, DUT responds at prior address 192.168.1.10
2722294	  5> *** The DUT delayed 298 ms to respond to the unicast ListIdentity command. The DUT shall not delay to a unicast ListIdentity request. Please verify the actual delay with a Wireshark capture.
2722326	  6> *** E.Int.F5.5 Change IP Address - failure logged
2730629	  1> *** The DUT delayed 314 ms to respond to the unicast ListIdentity command. The DUT shall not delay to a unicast ListIdentity request. Please verify the actual delay with a Wireshark capture.

** Warnings **

169	  1> ** Warning: Received UDP response from 192.168.1.4.
180	  2> ** Warning: Received UDP response from 192.168.1.5.
207	  3> ** Warning: Received UDP response from 192.168.1.4.
212	  4> ** Warning: Received UDP response from 192.168.1.4.
223	  5> ** Warning: Received UDP response from 192.168.1.4.
228	  6> ** Warning: Received UDP response from 192.168.1.4.
239	  7> ** Warning: Received UDP response from 192.168.1.4.
250	  8> ** Warning: Received UDP response from 192.168.1.4.
261	  9> ** Warning: Received UDP response from 192.168.1.4.
272	 10> ** Warning: Received UDP response from 192.168.1.4.
283	 11> ** Warning: Received UDP response from 192.168.1.4.
316	 12> ** Warning: Received UDP response from 192.168.1.4.
321	 13> ** Warning: Received UDP response from 192.168.1.4.
333	 14> ** Warning: Received UDP response from 192.168.1.4.
338	 15> ** Warning: Received UDP response from 192.168.1.4.
2428726	  1> ** Warning: No data in the Data attribute. Please verify if it's acceptable.
2433224	  1> ** Warning: No data in the Data attribute. Please verify if it's acceptable.
2709015	  1> ** Warning: 67 I/O packets (Sequence Number: 240, 244, 248, 251, 256, 259, 263, 266, 270, 275, .........................................................) generated by the DUT does not match the API 20 ms. 
2709044	  2> ** Warning: 59 I/O packets (Sequence Number: 2, 5, 9, 13, 17, 24, 28, 32, 35, 39, .................................................) generated by the DUT does not match the API 20 ms. 
2709288	  3> ** Warning: 2 I/O packets (Sequence Number: 2, 3, ) generated by the DUT does not match the API 20 ms. 
2709360	  4> ** Warning: 96 I/O packets (2, 5, 9, 13, 16, 20, 24, 28, 31, 35, ......................................................................................) generated by the DUT does not match the API 20 ms. 
2709401	  5> ** Warning: 36 I/O packets (Sequence Number: 373, 378, 381, 385, 389, 392, 396, 400, 404, 408, ..........................) generated by the DUT does not match the API 20 ms. 
2709431	  6> ** Warning: 136 I/O packets (Sequence Number: 2, 5, 9, 12, 16, 19, 24, 27, 31, 39, ..............................................................................................................................) generated by the DUT does not match the API 20 ms. 
2709775	  7> ** Warning: 1 I/O packets (430, ) generated by the DUT does not match the API 20 ms. 
2709824	  8> ** Warning: 119 I/O packets (Sequence Number: 54, 59, 62, 66, 70, 73, 77, 82, 85, 90, .............................................................................................................) generated by the DUT does not match the API 20 ms. 
2709853	  9> ** Warning: 11 I/O packets (Sequence Number: 2, 6, 10, 14, 17, 21, 25, 29, 32, 36, .) generated by the DUT does not match the API 20 ms. 
2710097	 10> ** Warning: 2 I/O packets (Sequence Number: 2, 3, ) generated by the DUT does not match the API 20 ms. 
2710169	 11> ** Warning: 47 I/O packets (2, 6, 10, 13, 17, 21, 25, 28, 32, 36, .....................................) generated by the DUT does not match the API 20 ms. 
2710210	 12> ** Warning: 86 I/O packets (Sequence Number: 188, 192, 196, 199, 203, 207, 210, 214, 218, 222, ............................................................................) generated by the DUT does not match the API 20 ms. 
2710239	 13> ** Warning: 140 I/O packets (Sequence Number: 1, 5, 9, 12, 16, 20, 24, 27, 31, 34, ..................................................................................................................................) generated by the DUT does not match the API 20 ms. 
2710483	 14> ** Warning: 2 I/O packets (Sequence Number: 2, 3, ) generated by the DUT does not match the API 20 ms. 
2828673	  1> ** Warning: The Max Instance attribute did not changed after receiving a LLDP frame from a new interface. The DUT reuses previous instance number?

* Reminders *

2707436	  1> * Reminder:  The DUT supports Large_Forward_Open service, please run LFW test separately.
2722083	  1> * Reminder: Device support of EtherNet/IP ACD (Address Conflict Detection) requires manual verification.  Please contact ODVA for assistance.
2749542	  1> * Reminder: A complete automated Behavior test for DLR Object is not included in this version. Successfully passing the manual test procedure will waive this error.
2758882	  1> * Reminder: An automated Behavior test for QoS Object is not included in this version. Successfully passing the manual test procedure will waive this error.
2770429	  1> * Reminder: An automated Behavior test for Time Sync Object is not included in this version. Successfully passing the manual test procedure will waive this error.
2783927	  1> * Reminder: The DUT supports the new Identification TLV.